How can we help you today?

PME all versions - Log Inserter won't open in Designer if a Log Acquisition Module (LAM) has too many inputs

Product Line:

Power Monitoring Expert all versions
_____________________________________________________________
Environment:

Designer

_____________________________________________________________
Issue :

Log Inserter won't open in Designer if a Log Acquisition Module (LAM) has too many inputs

In Designer, you will see a 'communications error' dialog. In the system log you will see this error:
Image
_____________________________________________________________
Proposed Solution:
There is a certain limitation on the number of inputs can be connected to a Log Acquisition Module. Try to reduce the number of inputs to below 1500 per Log Acquisition Module. Add a second Log Acquisition Module if further inputs are required.

Schneider Electric Egypt and North East Africa