When configured with multiple vSAN clusters, PowerChute Network Shutdown fails to disable HA and vCLS all the clusters.
Issue:
PowerChute Network Shutdown has been configured to shutdown multiple vSAN clusters and HA/vCLS is only disabled on one cluster.
Product Line:
PowerChute Network Shutdown versions 5.0, 5.1, 5.2
Environment:
VMware vCenter 7 or 8 configured with multiple vSAN clusters.
Cause:
PowerChute can only disable HA and power off vCLS for a single cluster.
Solution:
Install multiple instances of PowerChute. One for each cluster.
Released for: Schneider Electric Egypt and North East Africa