Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do I setup the OFS Server as a service on Windows Server 2022?

Issue:

Running OFS server as a service on Windows Server 2022


Product Line:

OFS server


Resolution:

To run OFS Server as a service follow the steps below...

  1. Install the OFS Server on the PC
  2. Run the ofsservice.bat file located in C:\Program Files (x86)\Schneider Electric\OFS\Server

note: with OFS Server V3.63 SP3, the batch file is not created automatically with the installation of the server. You must create it manually in the

C:\Program Files (x86)\Schneider Electric\OFS\Server directory. To create the batch file, create a new text document and rename it to ofsservice.bat then edit the file and enter the command

"regofsservice /true" in the file and save the file.

image1

3. Check to make sure the service is created as shown below. You can change the startup mode to automatic and start the service

image2

4. The server must be setup in the DCOM configuration. Type in dcomcnfg in the search on the tool bar to enter the DCOM configuration. Look for the Schneider-Aut OPC factory server, right click and select properties image3

5.  Under the general tag, select Connect as the Authentication Level

image4

6. Under the Identity tab select this user and enter the login user credentials then select apply and ok

image5

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: