Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the maximum number of Battery Modules supported by the number of Power Modules installed in a Smart-UPS Modular Ultra?

Issue:

What is the maximum number of Battery Modules supported by the number of Power Modules installed in a Smart-UPS Modular Ultra?

Product Line:

APC Smart-UPS Modular Ultra 5-20kW

Environment:

All models and serial numbers

Resolution:

An APC Smart-UPS Modular Ultra 5-20kW (UPS Frame) is capable of handling external battery frames (XR Frames) with additional BMs (Battery Modules). However, the number of battery modules it can support is limited by the number of PMs (Power Modules) present in the system.


If the maximum number of battery modules is exceeded, the power modules will not be able to supply enough power under all conditions to properly charge the battery modules.


There are 6 slots in the UPS frame and the maximum number of battery modules in the UPS frame is 6 minus the number of power modules installed.


Please refer to the table below for more information.

No of PMsMax BMs SupportedMax BMs in UPS FrameMax BMs in XR FramesNo of slots in XR FramesMax supported XR Frames
1135842
22041644
32732446
42622446
52512446

Should you have further concerns, please contact us at https://www.apc.com/us/en/support/