How can we help you today?

IGP10-A/IGP20-A Re-range

EGU LRV = 4 mA Value

EGU URV = 20 mA Value

  1. Press the NEXT button twice and the word CONFIG will be displayed.
  2. Press ENTER and OUT DIR will be displayed
  3. Press NEXT 4 times and DISPEGU will be displayed
  4. Press ENTER and USE EGU will be displayed
  5. Press ENTER and EGU SEL will be displayed
  6. Press ENTER and the current engineering unit will be displayed
  7. Press NEXT until the desired engineering unit is displayed (i.e. FtH2O, inH2O, PSI...)
  8. When desired engineering unit is displayed, press ENTER and EGU LRV will be displayed
  9. Press ENTER and the cursor at the left side of the display will flash.
  10. Press ENTER and the left hand most digit will flash.
  11. Press NEXT until this digit matches the value of the most significant digit of the desired LRVvalue. Repeat procedure for the remaining 3 digits until the entire LRVvalue has been entered
  12. Press ENTER and SET DP will be displayed
  13. Press NEXT until the decimal point is in the correct location
  14. Press ENTER and EGU URV will be displayed.
  15. Press ENTER and flashing cursor will appear at the left side of display
  16. Press ENTER and the left most digit will flash
  17. Press NEXT until this digit matches the value of the most significant digit of the desired URVvalue. Repeat procedure for the remaining 3 digits until the entire URVvalue has been entered
  18. Press ENTER and SET DP will be displayed
  19. Press NEXT until the decimal point is in the correct location
  20. Press ENTER and CANCEL will be displayed
  21. Press NEXT and SAVE will be displayed
  22. Press ENTER and device will be returned to Measurement Display
  23. Complete

Schneider Electric Egypt and North East Africa
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
Help Center

Help Center