Smart UPS Ultra - Experiences a System Braindead / Battery Pack Is Not Compatilble
Problem:
- Battery Pack is not compatible
- P08, P11, P16 and P19 alarms (pre-charger damage)
- G03 alarm (logic power supply alarm)
- System Brain Dead
- Battery lost communication
Product Line: SRTL3KRM1UWC, SRTL3KRM1UIC, SRTL2K2RM1UWC, SRTL2K2RM1UIC, SRTL3KRM1UC, SRTL2K2RM1UC, SRTL3KRM1UWNC, SRTL3KRM1UINC, SRTL2K2RM1UWNC, SRTL2K2RM1UINC, SRTL3KRM1UNC, SRTL2K2RM1UNC
Environment: All Serial Numbers
Cause
The power factor correction (PFC) circuit is experiencing sagging current at higher input voltages (>240VAC), leading to defects in logic power and causing the system to become brain dead. Additionally, battery timing and traffic congestion are contributing to system mismatches
Resolution:
Firmware ID1062 and ID1063 v4.9 has been released and addresses this issue as well as the following
1. Improve PFC sagging current when input voltage is larger than 240V.
2. Reduce input peak current at on‐line transient moment when input voltage is larger than 240V.
3. When a fault is detected during self‐test, prevent turning on PFC and transfer to failure bypass mode.
4. Force battery to sleep while UPS is in fault to avoid consuming battery energy.
5. Adjust the fan control algorithm for reducing noise.
The firmware can be downloaded here - https://download.schneider-electric.com/files?p_Doc_Ref=Smart-UPS_FW_Release_Notes&p_enDocType=Firmware&p_Archive_Name=Smart-UPS_FW_Release_Notes.zip
Released for: Schneider Electric Egypt and North East Africa
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.