Easy-UPS BVG AVR Details
The Automatic Voltage Regulation (AVR) details for the Easy-UPS BVG range are:
Boost: 18% - This will be activated when the input voltage is 207 VAC or below.
Trim: 15% - This will be activated when the input voltage is 253 VAC or above.
Released for: Schneider Electric Egypt and North East Africa