How can we help you today?

What are the differences between Harmony P6, Harmony FP6 and Harmony P6 HMI utility installers?

Issue:
The user needs to know the differences between Harmony P6, Harmony FP6 and Harmony P6 HMI utility installers.

Product:
Harmony P6 IPC series

Environment:
Drivers installation / Updates

Answer:

- Harmony P6 and Harmony FP6 utility installer
This installer includes dedicated utilities such as Buzzer, Brightness control, and others
Please find the latest version: "Harmony P6 - Software and Firmware"
- Harmony P6 HMI utility
This is a special utility for replacing Harmony P6 basic model from HMIG5U21/HMIG5U22.
HMIG5U21/HMIG5U22 have dedicated utilities, but Harmony P6 doesn't support these dedicated utilities as default.
If customer installs this utility, customer can only use some dedicated features (but not all).

Schneider Electric Egypt and North East Africa