Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the Maximum capacity of the SURT013?

Question:

What is the Maximum capacity of the SURT013 equipment cart?

Product Line:

SURT013

Environment:
Smart-UPS UPS

Solution:

The maximum recommended capacity of the SURT013 is 550Lbs based on its design. While the cart has 4 pieces of 650 lbs rated casters but we do not suggest exceeding the 550 limit. The limit takes the cart's weight and includes a safety buffer to accommodate dynamic load weight when in motion. Installing  equipment that exceeds this weight  may cause damage to equipment or may result to injury.

Unit is made specifically for the  SURT15KRMXLT and SURT20KRMXLT using it with other equipment is not recommended.

SURT15KRMXLT and SURT20KRMXLT UPS units may be stacked to a total height of not more than 18U on its own on the floor without the cart. But when using cart only UPS and First Battery pack should be installed and additional accessories such as additional External packs , Stepdown Transformers should be installed in a separate cart.

Here are the UPS supported and  Battery packs and their weight.

  • SURT15KRMXLT - 546.15 lbs(US) (247.73 kg)
  • SURT20KRMXLT  - 546.15 lbs(US) (247.73 kg)
  • SURT192RMXLBP2 - 400.84 lbs(US) (181.82 kg)

Here are some SURT15KRMXLT and SURT20KRMXLT configuration bundles that when installed Needs to be split in multiple carts because it exceeds weight capacity.

  • SURT15KRMXLT-TF5 - 641.35 lbs(US) (290.91 kg)
  • SURT20KRMXLT-TF5 - 641.35 lbs(US) (290.91 kg)

Image shows SURT013 Equipment Cart with no load

If you have any clarifications or concerns, please do contact us at 1-800-800-4272 or chat with our Technical Support Agents.

*Attached on this article is the user guide that shows top and bottom Image of cart and shows in detail how the UPS is mounted and installed on equipment cart.

Schneider Electric Egypt and North East Africa

Attachment(s)
SURT013 User Guide.pdf [90.81 KB]
Explore more
Range:
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
Product: