How can we help you today?

How can you save the ATV320 Drives program with function blocks using the Multiloader device?

Issue:

Saving the ATV320 Drives program with function blocks on the Multiloader programmer.

Product Line:

ATV320 with Multiloader device.

Environment:

All

Cause:

Getting an error message when trying to download the ATV320 program with function block using the multiloader.

Resolution:

When the ATV320 has ATVLogic running, you must stop the ATVLogic running before any multiloader transfer (you must set fbCd=STOP via keypad using ATV320 integrated Jog dial). Otherwise, the transfer will not be done.

Menus

-Config

-Full

-Function blocks

-FB command (fbCd)

set to Stop.

Now you can download the ATV320 program into the Multiloader.

Schneider Electric Egypt and North East Africa