Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
PME 2024, 2024R2: EPSS report subscription throws deserialize argument error

Environment:

Power Monitoring Expert 2024 and 2024R2

----------------------------------------------------------------------

Product Line:

EPSS Report

----------------------------------------------------------------------

Description of the issue:

After upgrading from an older version of PME, a saved EPSS report subscription throws a deserialize argument error as it is shown in the attached screenshots below.

Image

Image

Image

----------------------------------------------------------------------

Cause:

The EPSS report template includes some new parameters that were not present in the older versions of PME. So, when the subscription runs and it references the new template, it finds missing parameter data. This causes a deserialization error.

Workaround:

Open the saved report in Web Reporter and re-save the same report. This will add all the missing parameters.