How to power cycle an InRow unit Generation 1?
Issue:
How to power cycle an InRow unit Generation 1?
Product Line:
InRow Family Gen1.
Environment:
ACRD1XX, ACRD2XX, ACSC1XX, ACRC1XX, ACRD5XX, ACRP1XX, ACRP5XX, etc.
Cause:
General aid for Customers.
Resolution:
- Please put the unit into StandBy mode (Figure 1), you might be required to input the password, use the default oneà apc (lower case).
Figure 1
- When the fans start ramping down, please unplug the dedicated power cord(s) to the unit (It can be top or bottom fed) [Figure 2] or put down the dedicated breaker(s) to the unit (If it’s hard-wired), or if it’s a 600mm InRow (Figure 3) and leave the unit without any power for at least 5 minutes.
Figure 2 (For 300mm InRow only).
Figure 3 (For 600mm InRow only).
- After the 5 min passes, restore the power to the unit, allow a couple of minutes, for the display to pop up, change the mode from StandBy to On (Figure 4), and test the proper operation of the unit.
Figure 4
NOTE: This process can only be executed from the front display of the unit.
Released for: Schneider Electric Egypt and North East Africa
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
Help Center
Find support resources for all your needs, in one place.