Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to Retrieve Dump Files From a SCADAPack x70 RTU?

Dump files will be created if an unexpected exception occurs on the SCADAPack x70 RTU.

There are two methods to retrieve the dump files from the SCADAPack x70 RTU.

  1. Using the FTP feature.
  • In RemoteConnect, enable Telnet and FTP server options.

Dump1

  • Connect to the SCADAPack x70 RTU using PuTTY or some other command line interface tool.
  • At the command prompt, type dir to confirm the names of the dump files created.

Dump2

  • Use ftp to transfer the dump files from SCADAPack x70 RTU to PC directory.

Dump3

  1. Using Read File from Device feature.
  • Go online with the SCADAPack x70 RTU using RemoteConnect.
  • Right click on SCADAPack x70 Controller Settings -Device DTM>Additional Functions>Read File from Device

Dump4

  • Type the name of the dump files in the Source File that need to be read and the destination or directory where the files are to be saved, then click OK button.

Dump5