Time sync from PME to TransferPact Active Automatic, EM3570 device causing 1 hr difference in timestamp
Environment:
Power Monitoring Expert 2023, 2024, 2024R2
----------------------------------------------------------------------
Product Line:
TransferPact Active Automatic, EM3570
----------------------------------------------------------------------
Description of the issue:
- Connect a TransferPact Active Automatic or EM3570 in the Management Console.
- Check the time sync with PME.
----------------------------------------------------------------------
Workaround:
- Open the .XML file for that device type, either from the config\translator folder if using a modified file or from the system\translator folder.
- Change the DeviceTimeLocale to "Local" in the XML file as shown in the attached screenshot below.
- Restart the ION Network Router service.
Released for: Schneider Electric Egypt and North East Africa