Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to change decimal resolution (2 digits, 3 digits, 4 digits ect) in PME Estidama gadget Period over Period graph.

Environment:

Power Monitoring Expert 2022, 2023, 2024

----------------------------------------------------------------------

Product Line:

Estidama gadget.

----------------------------------------------------------------------

Description of the issue:

If the customer wants to change the decimal resolution of the displayed value in this gadget, then how can they do that.

----------------------------------------------------------------------

Workaround:

It can be done by editing the "EstidamaPeriodOverPeriod.JS" JavaScript file from the folder mentioned in step 1.

Step 1:

Please edit EstidamaPeriodOverPeriod.JS file from the below location and change the precision value accordingly based on the requirement.

“C:\Program Files (x86)\Schneider Electric\Power Monitoring Expert\Applications\Dashboards\Content\Gadgets\EstidamaPeriodOverPeriod”

Please refer to the below snapshot to modify the precision value.

Image 1

eg:  Customer can change the precision from 3 to 2 if the customer wants to show 2 decimal values in the report.

Step 2:

Please ensure that the program file path may be different in your installation. Help yourself to find the PME installation path, and edit the java script file.

Step 3:

Once modified, just refresh the browser.