How can we help you today?

How do I run a battery test from the Web Interface in my Galaxy VS?

Issue: ​

Customers would like to use the web interface to run a battery test remotely.

Product Line:​

Galaxy VS

Environment:​

Galaxy VS (All versions)

Cause:​

Battery test is not available in the web interface

Resolution:​

The Remote Battery Test feature has been introduced in Firmware revision 6.118.3.171 (Released in May 2025) and is also available in higher versions. However, this function is not available by default in the UPS configuration.

This feature has to be enabled from the UPS display by following the path Configuration -- Battery -- Go to the second screen -- Battery Self-test allow remote control and checking the box.

Battery Configuration screen for Remote Battery Test



Once the setting is accepted, log in to the web interface. You will be able to see a new tab called Tests, where you can start a remote battery test.

Screen after enabling the remote battery test

Important note: Our commitment is to deliver secure products, utilizing secure development processes, and reliable update management; therefore, firmware upgrades can only be performed by Schneider Electric-qualified personnel during maintenance visits (repair or PM) and will not be posted on the website.

Secure NMC System for 3-Phase products can be consulted for further questions.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center