Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Using the Advanced Modbus Driver and Modbus Slave Driver in Geo SCADA Expert - SDE example

Using the Advanced Modbus Driver and Modbus Slave Driver in Geo SCADA Expert

Overview

This article provides a practical example of how to use both the Advanced Modbus Driver and the Modbus Slave Driver in a Geo SCADA Expert (GSE) environment. It is designed to help users quickly get started with Modbus communication simulation using a pre-configured setup.

The example includes an .SDE file that can be imported into a GSE 2020 or newer application. It demonstrates local Modbus TCP communication, requiring that port 502 is available on the host system.

Note: Configuration details for both drivers are available in the official Geo SCADA Expert documentation. This article focuses on demonstrating a working example for testing and learning purposes.

Getting Started

1. Importing the Example

• Import the provided .SDE file into the top level of your GSE application ($Root).
• This will create a structured set of objects, including a mimic for testing and monitoring.

2. Accessing the Mimic

• Navigate to the mimic: Modbus Master Slave Test.~Overview
• Switch the mimic to Runtime mode.
• You can now interact with the interface to simulate and observe Modbus communication.

What the Mimic Shows

Mimic

The mimic provides:
• Real-time communication status for both the Advanced Modbus and Modbus Slave drivers.
• Input fields to manually enter values for testing.
• Live feedback on how values are transmitted and received between the master and slave.

This setup allows users to:
• Validate driver configurations.
• Simulate real-world Modbus TCP communication.
• Modify object properties to test different scenarios.

Next Steps

Once the example is running:
• You can modify object properties (e.g., polling rates, register mappings, data types) to suit your testing needs.
• Use this setup as a template for building more complex Modbus integrations.
• Explore how changes in the master affect the slave and vice versa.

Conclusion

This example provides a simple yet powerful way to explore the capabilities of the Advanced Modbus and Modbus Slave drivers in Geo SCADA Expert. By using the included mimic and configuration, users can quickly simulate communication, test configurations, and gain confidence in deploying Modbus-based solutions.

Schneider Electric Egypt and North East Africa

Attachment(s)
Modbus Master and Slave example.sde [36.41 KB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: