EtherNet/IP Support for Smart-UPS
Issue:
EtherNet/IP Support for Smart-UPS with an NMC3
Cause:
Smart-UPS (SU) firmware v3.4 has added support for the EtherNet/IP protocol for certain SmartUPS models
Product Line:
Network Management Card 3 (NMC3) - AP9640, AP9641, AP9643
Solution:
EtherNet/IP (Ethernet Industrial Protocol) is an industrial networking protocol that enables communication between devices in automation and control systems. It is built on standard Ethernet and TCP/IP technologies and is widely used in manufacturing environments for real-time data exchange between programmable logic controllers (PLCs), sensors, actuators, and other industrial equipment.
As of Smart-UPS NMC firmware version 3.4 (SU), the EtherNet/IP protocol is supported on all Smart-UPS models with prefix SMT, SMX, SURTD, and SRT. In addition, the following Smart-UPS models are also supported (where other SRC models are not supported): SRC2KUXI, SRC3KUXI, and SRC3KUXIX709.
Released for: Schneider Electric Egypt and North East Africa