How can we help you today?

How to connect to the BMENOC0302(H) IPsec website

The BMENOC0302(H) IPsec website credentials are the following :

  • username: loader
  • password: Use the firmware password set in the EcoStruxure Control Expert application.
    For more information, refer to Firmware Protection topic in the "EcoStruxure Control Expert
    Operating Modes" guide.

Please note that In the documentation "Modicon M580 BMENOC0302(H) High Performance Ethernet Communication Module Installation and Configuration Guide Original instructions (NNZ44174.00) " in page 131, it is written that the username is modbususer, this will be corrected very soon in the next technical publication release

BMENOC0302 credentials from installation guide to be changed

Schneider Electric Egypt and North East Africa
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
Help Center

Help Center