How can we help you today?

ETE - FAQ - Offer: Can I trust EcoStruxure Transformer Expert technology?

The technology was built upon a foundation of over a decade of research conducted by the University of Queensland researchers, collaborating with four of Australia’s largest distribution and transmission utilities. It is based on peer-reviewed research and is verified by testing and data gathered from a large number of transformers.

Academic papers describing the methodology and white papers explaining the use of the EcoStruxure Transformer Expert methodology are available in Academic Papers.

Schneider Electric Egypt and North East Africa