Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
ETE - FAQ - Transformer: What is the effect of high moisture content in the transformer oil?

As the level of moisture content increases in a transformer, it has two major effects. Firstly, the additional water interacts with the paper in the insulation causing accelerated damage. This damage weakens the mechanical strength of the paper, allowing cracks to form and breakdowns to occur. Secondly, the additional water interferes with the insulation performance of the oil-impregnated paper. Under certain circumstances, this can result in insulation breakdown and catastrophic damage. Therefore, a high value of moisture in the transformer oil indicates an unsafe operating state. Such transformers must be managed very carefully and typically cannot be used to their original design limits safely.

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center