Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
ETE - Knowledge - Transformer: Improving the Determination of Water Content of Power Transformer Insulation Paper near the End of Its Functional Life

Many utilities use cellulosic adsorption isotherms to calculate the water content of transformer paper insulation from the water activity of the oil. However, a problem is that this method becomes less precise as the paper degrades because the adsorption isotherms change, and thus the water content of the paper derived from the water content of oil is no longer accurate. When this inaccuracy becomes significant, should the water activity, or the water content of paper, be used to estimate life remaining? In this article, a discussion is given on why the rate of degradation of paper is dependent on water activity, and the potential inaccuracies when using only water content of paper.

Paper: Improving the determination of water content of power transformer insulation paper near the end of its functional life

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center