Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
ETE - FAQ - Offer: Is EcoStruxure Transformer Expert suitable for new or refurbished transformers?

EcoStruxure Transformer Expert is suitable for new transformers, provided that Water Content of Paper (WCP) graphs are not utilized in the first 6 months of the transformer's life.

The WCP is estimated over time using Schneider Electric's Diffusion Model, which takes into account moisture mass flow in the model. This is done based on a finite-difference model which calculates the movement of moisture from the oil to the paper and deeper through layers of paper. This model requires moisture in oil to reach relative equilibrium with the moisture in the paper insulation. This process for new oil takes up to 6 months to stabilize. During this time, WCP graphs may not be accurate.

Schneider Electric Egypt and North East Africa

Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center