How can we help you today?

Is there protection recommendation with fuse for the input channels on TM3AI4?

Issue:

What protection is needed for the input channels on TM3AI4 from overcurrent or overvoltage?

Product Lines:

TM3

Environment:

PLC software configuration in EcoStruxure Machine Expert

Resolution:

There is no protection recommendation with fuse for the Input channels except the use of shielded cables and the connection of the shield to the FE:

Shield cable

Schneider Electric Egypt and North East Africa
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
Help Center

Help Center