Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Smart-UPS Ultra 5-10kW "EPO Activated" cannot be immediately cleared on the UPS LCD display

Issue: The "EPO Activated" alarm cannot be immediately cleared on the UPS LCD display

Product line: Smart-UPS Ultra 5-10kW models

Reason: If the UPS is turned on using the the System Enable Switch, it will immediately report an "EPO activated" alarm on the LCD display. This alarm must be manually cleared on the UPS LCD display before the UPS output can be turned on.

If this alarm is not cleared within ~10 minutes, the UPS may go in a standby state where subsequent attempts to clear the alarm may not clear it immediately.

Resolution: Perform several attempts to clear the alarm on the LCD display. By the 7th attempt, the alarm condition should clear, and UPS will be able to be turned on.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center