Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is there a hot-fix for Control Expert v15.3 to support the BMXXBP1600?

ISSUE

Support of BMXXBP1600


ENVIROMENT

Control Expert


HARDWARE

BMXXBP1600


RESOLUTION

The BMXXBP1600 is not supported with Control Expert v15.3. You will need to upgrade to v16.0 or later. There is no update for earlier versions.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: