How can we help you today?

How many wireless batteryless push buttons(ZBRT1/ZBRT2) can be connected to the EcoStruxure Panel server?

The maximum number of devices that are compatible with the EcoStruxure Panel server depends on the panel server version. PAS400 is compatible with max of 20 pushbuttons. The PAS600* and PAS800* versions are compatible upto100 wireless batteryless pushbuttons.

Schneider Electric Egypt and North East Africa