Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can I change the channel of ZBRA1 during commissioning with the EcoStruxure Panel server?

No, ZBRA1  only supports channel 11.  That is why you should set the radio channel to 11 on the EcoStruxure Panel server while commissioning with ZBRT1/ZBRT2, if you want to use ZBRA1.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: