Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Displaying Time Intervals in Hours, Minutes and Seconds on a Geo SCADA Mimic

Displaying Time Intervals in Hours, Minutes and Seconds on a Geo SCADA Mimic

Overview

In Geo SCADA Expert, it is common to work with points that represent elapsed time in seconds. However, displaying this raw value directly on a mimic can be difficult to interpret at a glance. To improve readability and user experience, you can format this value into a more intuitive hours, minutes and seconds (nnH nnM nnS) format using a Text object.

This article explains how to configure a Text object on a mimic to display a time interval in a human-readable format using built-in animation properties.

Objective

To convert and display a numeric value representing elapsed time in seconds into a formatted string showing hours, minutes and seconds (e.g., 1H 23M 45S).

Configuration Steps

1. Add a Text Object to the Mimic

• Open the mimic in Design Mode.
• Insert a Text object where you want the formatted time to appear.

2. Set the Animation Properties

• Open the Animations tab for the Text object.

Property Settings:

• Property: Format
Set this expression to 'Long Period' (including the single quotes).
This tells Geo SCADA to interpret the value as a time duration and format it accordingly.

• Property: Value
Set this expression to the point that contains the number of seconds you want to display.
For example: MyDevice.SecondsElapsed

Example Use Case

Imagine a point named Pump1.RunTimeSeconds that tracks how long a pump has been running. To display this on a mimic:
1. Add a Text object.
2. Set the Value to “.RunTimeSeconds” (using relative reference in this example).
3. Set the Format to 'Long Period'.

Expressions

The mimic will now show the run time in a format like 2H 15M 30S instead of just 8130 seconds.

Visual Example

A well-designed mimic might include:
• A numeric display showing the raw seconds.
• A formatted display showing the same value as a time interval.

Example

This dual representation helps operators quickly understand both the raw data and its practical meaning.

Conclusion

Using the 'Long Period' format in a Text object is a simple yet effective way to enhance the readability of time-based data in Geo SCADA Expert. It allows operators to interpret elapsed time more intuitively, improving situational awareness and decision-making.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center