Is a recovery USB available for PSA6 ?
No, recovery USB is not available to be purchased.
The user can create a recovery USB from the Recovery Utility feature provided on the HMIPSA6 Launcher.
Prepare a commercially available USB memory with a size of 32 GB or more, to create a recovery USB and follow the steps below:
- 1. Disconnect all connected devices from the product.
- 2. Insert a commercially available USB memory.
- 3. Open the Launcher on the desktop.
- 4. Select the Recovery USB icon.
- 5. Select the USB memory in Select a disk menu.
- 6. Select Start.
- 7. In the confirmation screen, select OK.
- 8. When completed, select OK.
Released for: Schneider Electric Egypt and North East Africa
Need help?
Product Selector
Quickly and easily find the right products and accessories for your applications.
Get a Quote
Start your sales enquiry online and an expert will connect with you.
Where to buy?
Easily find the nearest Schneider Electric distributor in your location.
Help Center
Find support resources for all your needs, in one place.