Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is the battery replaceable in PSA6?

Yes, the battery is accessible under the maintenance hatch and It can be replaced by the user.

Please use only CR-2032 lithium metal battery for the replacement (CR-2032 by Maxell is recommended).

Before opening the maintenance hatch, make sure to follow these steps:

  1. Disconnect the power supply from the product.
  2. Touch the housing or ground connection (not the power supply) to discharge any electrostatic charge from your body.
  3. Place the product face down on a clean, flat, level surface.