Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is CPU over-clocking with Turbo-boost available for PSA6?

Yes, the default setting is Turbo-boost enabled. It can be disabled from the BIOS menu.

When Turbo-boost is turned on for PSA6 with Core i5 CPU, it is recommended to use a power supply with at least 80% higher capacity than the specified power consumption.