Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is a recovery USB available for PSA6?

No, recovery USB is not available to be purchased.

The user can create a recovery USB from the Recovery Utility feature provided on the PSA6 Launcher.

Prepare a commercially available USB memory with a size of 32 GB or more, to create a recovery USB and follow the steps below:

  1. Disconnect all connected devices from the product.
  2. Insert a commercially available USB memory.
  3. Open the Launcher on the desktop.
  4. Select the Recovery USB icon.
  5. Select the USB memory in Select a disk menu.
  6. Select Start.
  7. In the confirmation screen, select OK.
  8. When completed, select OK.