Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the BMXNOR0200H module's Ethernet communication be reset using IO_DDT (ETH_RESET)?

1. Issue
Some customers have reported that the online help in Control Expert suggests BMXNOR0200H supports Ethernet communication reset via IO_DDT (ETH_RESET). However, this functionality is not supported. The only available method to reset the Ethernet communication is through the module’s web interface.

2. Product Line

  • Module: BMXNOR0200H

  • Software: Control Expert

3. Environment

  • Operating System: Windows 10 / Windows 11

  • Software: Control Expert

  • Browser: Any standard browser used to access the module’s web interface

4. Resolution
After consultation with R&D, it has been confirmed that BMXNOR0200H does not support Ethernet reset via IO_DDT. The only supported method is through the web interface of the module.

Note:
No updates to the user manual are planned. It is recommended to use the BMENOR2200H (Advanced RTU module) instead, which supports Ethernet reset via Device DDT.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: