Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Does the Ecostruxure OPCUA Server Expert support extracted bits for Variables with data type INT16 or UINT16?

Issue:

Ecostruxure OPCUA Server Expert support of extracted bits for INT and UINT


Product Line:

Ecostruxure OPCUA Server Expert


Resolution:

As of V2.1.4904 it is possible to address an extracted bit <BitNumber> NodeId by concataining ".<BitNumber>" to the NodeID of the container.
For instance, to address the extracted bit 4 of a Variable with NodeID "s=0:M580!MyVar", address the NodeID "s=0:M580!MyVar.4"

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center