How can we help you today?

Frequency Reading Not Displayed During Testing

Issue:

The P3 relay does not show frequency readings during a real or virtual injection test.

Product:

PowerLogic™ P3 Relay

Environment:

Testing scenario using virtual or secondary voltage injection.

Cause:

The frequency is not measured if:

  • The maximum of the three phase-to-phase or phase-to-neutral voltages is less than 5.5 × (VT primary / VT secondary) (primary voltage reference).
  • The secondary voltage injection is less than 5.5 V.

This is a design condition to ensure accurate frequency measurement.

Resolution:

Increase the magnitude of the injected voltage during the virtual injection test. After raising the voltage above the required threshold, the frequency readings will appear as expected.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
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
Start your sales enquiry online and an expert will connect with you.

Where to buy?

Where to buy?

Easily find the nearest Schneider Electric distributor in your location.

Help Center

Help Center

Find support resources for all your needs, in one place.

  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center