Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Compact Flash (CF) Cards Spares for the C3414 CPU

Issue:
Need to identify the correct spare part number for the Compact Flash (CF) memory card used with the C3414 CPU.

Product:
C3414 CPU, SAGE RTU Series

Environment:

  • Systems using C3414 CPU
  • Requires Compact Flash memory card for operation or replacement

Cause:
The CF card is a required component for the C3414 CPU, and users need the correct part number for ordering or replacement.

Resolution:
The part number for the required CF memory card is C3414-S02-10001.
Description: COMP FLASH 1GB W/FW&WLIC.

Schneider Electric Egypt and North East Africa