Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the minimum clearance between phases and ground for the secondary side connections for Trihal Transformers?

Issue:
Minimum clearance between phases and ground for the secondary side connections for Trihal Transformers

Product Line:
Trihal Medium Voltage Transformer

Resolution:
For low voltage connections (< 1100 V), the standardized distances between phases are defined by standards IEC 1439 and IEC 60664-1.
For a nominal voltage of 1000 V, with an overvoltage category III (impulse voltage of 8000 V) and a pollution degree 3 (industrial environment), the minimum air gap between two conductors is 8 mm.

Distance between phases:
Minimum 8 mm

Distance between phase and ground:
Minimum 10 mm with an insulating screen
Minimum 21 mm in air

Please see attached file for reference

Schneider Electric Egypt and North East Africa

Attachment(s)
22.09.2025_LV_Distance_rev0.pdf [134.23 KB]