Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How do I perform the initial internal battery connection? | Back UPS PRO BX

Issue:

The Back UPS PRO BX model (BX850M/1000M/1350M/1500M) does not power on or begin charging when first connected.

Product Line:

Back UPS PRO BX

Environment

  • BX850M-LM60

  • BX1000M-LM60

  • BX1350M-LM60

  • BX1500M-LM60

Cause:

When purchasing a UPS from the Back UPS PRO BX family, it is necessary to perform the initial connection of the internal battery before operating the unit. If this step is skipped, the UPS will not function properly or begin charging its batteries.

Resolution:

To connect, disconnect, or replace the internal battery, follow the steps shown in the images below:

8 image

7 image

Schneider Electric Egypt and North East Africa