Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Loading GUI Files for firmware Versions in the SAGE Offline Editor tool

Issue:

User needs the GUI file for a specific firmware version when using the SAGE Offline Editor but cannot find this version available.

Product:

SAGE RTU

SAGE Offline Editor Tool

SAGE 2x00

SAGE 3030x

SAGE  4400

SAGE 14x0

Environment:

Offline configuration of SAGE RTU files requiring GUI files for specific firmware versions.

Cause:

The Offline Editor does not automatically include all GUI files for every firmware version. When a new firmware version is used, the tool prompts the user to provide the corresponding GUI file.

Resolution:

The SAGE Offline Editor remembers previously used firmware versions and their associated GUI files. When a new version is introduced, it will prompt the user to specify the required GUI file.

  • Instructions for loading the .GUI file are provided on the first page of the Offline Editor (scroll down to find them).
  • The .GUI file is located inside the _Firmware.tar.gz package within the Firmware Update package.
  • Steps:
    1. Extract the .GUI file from the _Firmware.tar.gz package.
    2. Place the file in a folder on your laptop.
    3. Use the Offline Editor to point to that GUI file following the instructions.
  • Once configured, the Offline Editor will remember that the specific version configuration requires the corresponding GUI file and will load them automatically.

1

After applying these steps, the customer should be able to successfully see the required GUI version .