Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
SAGE RTU Manuals for Internet Explorer Settings

Issue:

Configuration settings for different versions of Internet Explorer.

Product:

SAGE RTU (Remote Terminal Unit)

C3413 CPU

Environment:

SAGE RTU units running C3413 CPU (Green Board) Non-Secure

Internet Explorer versions 8, 9, 10, and 11.

Cause:

Users need specific configuration settings to ensure compatibility and proper functioning of the SAGE RTU with various versions of Internet Explorer.

Resolution:

The following documentation is attached in this article:

  • Config@web_IE8_settings_V1.1
  • Config@web_IE9_settings_V1.1
  • Config@web_IE10_settings_V1.1
  • Config@web_IE11_settings_V1.2
  • SAGE FW & IE Config

Schneider Electric Egypt and North East Africa

Attachment(s)
Config@web_IE8_settings_V1.1.pdf [585.6 KB]
Config@web_IE10_settings_V1.1.pdf [650.3 KB]
Config@web_IE11_settings_V1.2.pdf [676.68 KB]
Config@web_IE11_settings_V1.2.pdf [676.68 KB]
Config@web_IE9_settings_V1.1.pdf [629.97 KB]
SAGE FW & IE Config.pdf [361.59 KB]