Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
SAGE RTU Latest Firmware (Non-Secure Version)

Issue:

Users need access to the latest non-secure firmware available for SAGE RTU devices.

Product:

SAGE RTU, All models using a CPU C3413 (Green CPU Board)

Environment:

SAGE RTU units using C3413 CPU (Green board) in standard environments requiring updated firmware for compatibility and functionality.

Cause:

Users require the latest firmware to ensure compatibility and optimal performance of SAGE RTU devices up to the latest possible firmware for this hardware.


Resolution:

The latest Non-Secure firmware for SAGE RTU units is attached to this article for your reference.

It only applies to CPU C3413 (non-secure) versions.

Schneider Electric Egypt and North East Africa

Attachment(s)
c3413-500-001f0_pc_update_files.zip [6.04 MB]