Native Power Management of Smart-UPS with the SRTD prefix on Linux over USB.
Issue:
Smart-UPS models with the SRTD prefix may not be recognized as UPS/Batteries when connectedto Linux using a USB cable. The UPS is detected as a HID device (a hiddev* file is created in the /dev/usb/ folder, e.g., hiddev1), but the battery icon and subsequent power pages that appear for other UPSs are not showing in the Desktop.
Product Line:
Smart-UPS models Smart-UPS models with SKUs that start with SRTD2K2R2, SRTD3KR2, SRTD2K4R2, SRTDBP3KR2, SRTDBP2K4R2.
Environment:
Linux, USB connection.
Cause:
A 95-upower-hid.rules udev rules file contains a list of idVendor/idProducts of HID devices that upower (Linux power management) should manage, for example, on Red Hat:
# APC
ATTRS{idVendor}=="051d", ATTRS{idProduct}=="0000", ENV{UPOWER_BATTERY_TYPE}="ups"
ATTRS{idVendor}=="051d", ATTRS{idProduct}=="0002", ENV{UPOWER_BATTERY_TYPE}="ups"
ATTRS{idVendor}=="051d", ATTRS{idProduct}=="0003", ENV{UPOWER_BATTERY_TYPE}="ups"
Smart-UPS with the SRTD prefix has a new PID/Hardware ID (0005). This propagates to Linux distributions over time and may not be present in your distribution if the new PID/Hardware ID is not present in the 95-upower-hid.rules file, the device won’t be managed by upower and won’t appear as a battery/UPS.
You can find this file on Linux by executing the following command:
find / -name '95-upower-hid.rules' 2>/dev/null
Typical locations are:
/lib/udev/rules.d/95-upower-hid.rules
(Most common location for system-provided rules)
/usr/lib/udev/rules.d/95-upower-hid.rules
(Used by some distributions, especially those following newer filesystem hierarchies)
/etc/udev/rules.d/95-upower-hid.rules
(For local/admin overrides; if present here, it overrides the system version)
Resolution:
- Check if an updated file is available from upower:
- On Red Hat: run the commands
sudo yum update upower
or (on newer systems):
sudo dnf update upower
- On SUSE: run the commands
sudo zypper refresh
sudo zypper update upower
- If an update is not yet available, manually update the existing 95-upower-hid.rules file. Add a line for the new Product ID 0005 to your current 95-upower-hid.rules file:
# APC
ATTRS{idVendor}=="051d", ATTRS{idProduct}=="0000", ENV{UPOWER_BATTERY_TYPE}="ups"
ATTRS{idVendor}=="051d", ATTRS{idProduct}=="0002", ENV{UPOWER_BATTERY_TYPE}="ups"
ATTRS{idVendor}=="051d", ATTRS{idProduct}=="0003", ENV{UPOWER_BATTERY_TYPE}="ups"
ATTRS{idVendor}=="051d", ATTRS{idProduct}=="0005", ENV{UPOWER_BATTERY_TYPE}="ups"
Note: Future package updates may overwrite this change.
Released for: Schneider Electric Egypt and North East Africa