Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Is it acceptable to supply an external 24V, 1A source to the M241 PLC inputs?

Issue:

Can an external 24V/1A power supply be connected to the M241 PLC inputs?

Product Line:

M241

Environment:

All model numbers

Resolution:

It is acceptable to use a 24v / 1A external power supply for the PLC inputs.

But we have to include the protection such as fuses on each COM connections:

wiring

A: Sink wiring

B: Source wiring