How can we help you today?

What is our Salt Spray rating on a QED-2 Switchboard?

Subject:

Verification of QED2 Switchboard Paint Finish Standards
Issue:

Paint Standard – Humidity and Corrosion Resistance Testing
Product Line:

QED2 Switchboard
Environment:

Replacement Projects / Product Evaluation
Cause:

Product Design and Material Specifications

Resolution:
• Please refer to the attached PDF document, which includes the technical cut sheet for the paint used in QED2 switchboards.
• The document outlines the results of the 1,000-hour salt spray test, demonstrating compliance with corrosion resistance standards.
• This information can be used to verify finish durability in humid or corrosive environments.

Schneider Electric Egypt and North East Africa

Attachment(s)
Paint Std 2018 (3).pdf [183.58 KB]