Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Keyboard Latency When Using Virtual ViewX

Some customers may experience keyboard input latency when using Virtual ViewX while typing data into script generated text boxes.

This issue does not happen when typing in other dialog boxes, like the standard box generated by the "Control" method pick action or entering alarm filters, for example.

Currently the workaround is to add a file called "Thinfinity.params.ini" to the "C:\Program Files\Schneider Electric\VirtualViewX\bin32" folder of the Virtual ViewX folder. The file must contain the following:

[Options]
UseTimerService=0

Once the file is in place and the Virtual ViewX Server is restarted, the issue should be resolved.

Note: The workaround above was tested on Geo SCADA 2023 Build 86.9210.1 and newer. If using an older version, please first upgrade to 86.9210.1 or newer.

Schneider Electric Egypt and North East Africa

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: