How can we help you today?

PME - What are all of the mouse and keyboard combinations that can be performed in designer

Issue

The following table lists the different mouse and keyboard combinations you can perform on a module’s input or output symbols, and their corresponding functions:

Product Line

Power Monitoring Expert 8.2
Power Monitoring Expert 9.0
Power Monitoring Expert 2020
Power Monitoring Expert 2021
Power Monitoring Expert 2022
Power Monitoring Expert 2023
Power Monitoring Expert 2024

Environment

Designer

Cause

Many new users requested a visual representation of the mouse and keyboard combination that can be performed in designer

Resolution

table lists the different mouse and keyboard combinations you can perform in designer

Schneider Electric Egypt and North East Africa