Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Machine Expert Error: "Multiple mapping to an output is not allowed. Either the subelement or the parent already contains a mapping."

-> Issue:

Error: "Multiple mapping to an output is not allowed. Either the subelement or the parent already contains a mapping."

-> Product Line:

Machine Expert

-> Resolution:

Take this image as an example:

exampleimage

To solve the error, you have to delete the "qwIO_Out" WORD to be able to declare/write the BOOLS below.

The reason for that is for Safety Reasons:

-> If you assign a Symbol to the whole WORD of the outputs and you write like 11111111 11111111 binary to it, it will turn on all the Outputs pushing 24V on ALL the pins.

-> If you assign a Symbol just to Bit 0 (%QX0.0) of the outputs, and you set it to FALSE, then you push 0V on that Output Pin.

If you assign BOTH Symbols, what happens? It will be the last line of code that executes that "wins", but this causes unexpected behavior because the programmer may not know which line of code is first or even that BOTH writes exist.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team. If you are not located in North America, please contact your local Customer Care Center for assistance:Support | Schneider Electric Global (se.com)

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center