How can we help you today?

Why does my RemoteConnect project show conflicts and invalid entries after reading from a SCADAPackx70 RTU?

Question

After reading the RemoteConnect program from the SCADAPack 57x or 47x RTU, the program results in configuration conflicts when going online. It shows invalid entries in the object configuration.

Invalid entries


Answer

This issue occurs because the project was originally created using an older version of RemoteConnect that allowed invalid names. The current version enforces stricter naming rules and no longer permits these invalid entries.


Solution

To resolve this issue:

  1. Export the project to Excel from RemoteConnect.
  2. Search and replace all invalid names. For example:
    • Replace PH. with PH_.
  3. Import the updated file back into RemoteConnect.
  4. Verify that all invalid entries are corrected and configuration conflicts are resolved.

Schneider Electric Egypt and North East Africa

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Center