How can we help you today?

Where to Find the DTM Version Matrix for Control Expert v16.2 and Older Versions ?

Please refer to the DTM Version Matrix below, which corresponds to CE v16.2 and previous versions.

Control Expert Version
DTM Name14.014.0 Hotfix14.114.1 Hotfix15.015.0 SP115.115.215.316.016.2
BME NOC 03x1.x2.12.202.12.232.13.362.13.372.14.232.14.482.15.722.16.292.17.242.19.693.0.10.0
BME H58 x0402.12.202.12.232.13.362.13.372.14.232.14.482.15.722.16.292.17.242.19.693.0.10.0
BME P58 x0x02.12.202.12.232.13.362.13.372.14.232.14.482.15.722.16.292.17.242.19.693.0.10.0
BME H58 x040S2.12.202.12.232.13.362.13.372.14.232.14.482.15.722.16.292.17.242.19.693.0.10.0
BME P58 x040S2.12.202.12.232.13.362.13.372.14.232.14.482.15.722.16.292.17.242.19.693.0.10.0
NOC 78x002.12.72.12.72.13.322.13.322.14.112.14.262.15.242.16.122.17.112.19.132.21.40.0
NOC 78x00.22.12.72.12.72.13.322.13.322.14.112.14.262.15.242.16.122.17.112.19.132.21.40.0
M_NOC 04023.12.73.12.73.13.343.13.343.14.113.14.283.15.263.16.123.17.113.19.153.21.39.0
Advanced_Generic_EDS1.8.51.8.51.9.321.9.321.10.111.10.241.11.231.12.121.13.111.15.131.17.39.0
Generic_Device1.8.51.8.51.9.321.9.321.10.111.10.241.11.231.12.121.13.111.15.131.17.39.0
Modbus_Device1.2.51.2.51.2.51.2.51.2.51.2.141.3.21.4.01.5.01.7.21.9.39.0
BME CXM 01001.00.00031.00.00031.00.00031.00.00031.00.00031.00.00041.00.00071.00.00081.00.00081.00.00081.00.009
PME Generic DTM1.0.321.0.321.0.321.0.321.0.321.0.321.0.371.0.371.0.371.0.41(*)1.0.45
BME AHI 08121.1.71.1.231.1.71.1.71.1.91.1.121.1.201.1.201.1.201.1.221.1.23.0
BME AHO 04121.1.71.1.231.1.71.1.71.1.91.1.121.1.201.1.201.1.201.1.221.1.23.0
BME NOR 2200NANANA1.0.0611.0.0872.1.20353.13.0.22049.13.0.22055.13.0.22308.14.0.23311.24.1.24326.1
ModbusPlaceHolderNANANANA1.0.91.0.181.0.221.0.221.0.221.0.221.0.26
EIPPlaceHolderNANANANA1.0.91.0.181.0.221.0.221.0.221.0.221.0.26
EdgeIO DTMNANANANANANANANANANA1.1.25092.10

(*) Version 1.0.38 in V16.0.12192, and version 1.0.41 in V16.0.01261


Schneider Electric Egypt and North East Africa